Hi,
I have found that setting the RST pin low causes the power to be 110 mW lower
compared to when register 40h is set to power down everything except ADC and
OSC (D2h).
Shutting down everything using reg 40h uses 70mW more than a full reset using
the RTS pin.
Is there any way to reduce the power further without leaving the PCM9211 in
reset?  The design requires that the ADC is powered for level detection.
Any help would be appreciated. 
Thanks, 
Barabas