Dear Sir,
Questions:
1) In Status and Load Diagnostic Register 0x02, when the D4 bit (in a fault condition) will be set 1?
Does it relate to /FAULT pin? Means will be set 1 when /FAULT is active?
2) In Status and Load Diagnostic Register 0x02, will D4 bit set 1 when open speaker load happens?
3) What is the proper way to detect if there is speaker open load? Can only read bit D2 in load diagnostic register?
Thanks.
Best regards,
Chin