This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3101: Compatible with ADC3100

Part Number: TLV320ADC3101
Other Parts Discussed in Thread: TLV320ADC3100

Hi Team,

I find the ADC3100 said that "The TLV320ADC3100 is form-factor and software compatible with the TLV320ADC3101."

And so does ADC3101 to ADC3100?

Roy

  • Hi Roy,

    I'm not sure I 100% understand your question, but we'll explain some of the main similarities and differences.

    The ADC3101 and ADC3100 share the same pinout, register map, serial and Audio interfaces. 

    The ADC3100 offers a lessened feature set and does not have the programmable mini-DSP like the ADC3101 which is why the 1k pricing is lower on TI.com.