Other Parts Discussed in Thread: TAS5756M, TPA3156D2
Hi,
I have a question regarding this part (TPA3126d2). On my current project, I have to design a BT speaker who needs to drive 2 speakers (1 pair) of 6 ohms each, but it also should be able to drive 2 pairs (first pair in parallel with the second one), if the customer wants it. That scenario will give a 3 ohms load per channel. This part has a minimum load of 3.2 ohms on BTL mode, the question is; can I use it even though it will go a little bit under 3.2 ohms in some cases (when the customer connects 2 pairs of speakers in parallel)?
The audio requirements are:
- Total Harmonic Distortion (THD+N): 0.1% or less at rated power output
- Rated Power Output: 25 Watts per channel @ 6 ohms RMS (I chose a 50w/channel amp to make it work more relax, please advice if I can have a less powerful amp)
- Minimum load impedance: 3 ohms
- Power supply 22V (I can go up to 24V or 26V if needed, but no more than that)
If you think this part is not suitable for the purpose, please advise another part.
Best regards,
Guillermo