Part Number: SRC4382
I have 8 instances of the SRC4382.
The measured phase difference of the TX output pins (at the XLR end) between the 8 instances is mostly zero which is what I expect as the MCLK, LRCLK and BCK is the same for the 8 ICs. And the register setting is the same for all 8 ICs. However, sometimes, if I unplug one of the outputs, and re-plug, I get a phase difference of 75 degrees. What is the cause of this unexpected phase difference?
FYI, we are comparing the XLR outputs using a phase scope.
Thanks,