Other Parts Discussed in Thread: TLV320AIC3106
Dear all,
I designed a TLV320AIC34 board, and the TLV320AIC34 works in master mode. The GPIO2_A connects a external oscillator whose frequancy is 12.288MHz. I carefully ready TLV320AIC34's datasheet, especilly page 22. The CLKDIV_IN is connected with GPIO2_A, CLKOUT_IN is connected with CLKDIV_IN, M is set to 1, N is set to 2. By this configuration, I can see a wave whose frequency equals to 12.288M via GPIO1_A. The PLL_IN is connected to GPIO2_A, R is set to 1, P is set to 1, J is set to 8, D is set 0, the other configuration is default. Theoretically the sampling frequency is fs=(12.288e6*8*1)/(256*8*1)=48000 Hz. unfortunately, I can not see any signal from BCLK_A and BCLK_A. One more question, from Page 22, there is a switch denoted as CODEC_CLKIN, I can not find register that selects CLKDIV_OUT or PLLDIV_OUT.
The schematic and code are attached, can you help me to solve it. Thank you very much.TLV320AIC34.pdf