Other Parts Discussed in Thread: PCM2912,
I built an audio interface with a PCM 2902(E), about 7 years ago. Originally it worked with no problems. But with more recent PCs/versions of windows (eg more recent versions of WIndows 10) it would only record from one of the input channels and would route it to mono, i.e. the one working input channel would be recorded as the same in L and R, but it would "ignore" the other channel. As I am a mere hobbyist, I wondered about solder joint failure somewhere in the analog input signal path. I reflowed all the relevant solder joints with no change evident. I realised I also had a commercially made interface that used the PCM 2900. I found that, again, this would ignore one input channel and route the recording to mono. I tried the commercially made interface with a computer with an older version of windows 10 and it did work in both channels. I tried the home-made interface with an older version of windows 10 and, again, it also works in both channels. So it would appear that there is some issue with the windows 10 driver??