This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3221EVM: TPA3221: Output power doesn´t work (no EVM)

Part Number: TPA3221EVM


Dear team,
I'm designing amplifier with TPA3221 and I can't get the output power from it.

VCC = 20 - 30V
Vin = 2 Vpp
Zout = 8 Ohm
OTW = 5 V
FAULT = 5 V





I noticed that behind the capacitor (pin 8) is Vin + 4 Voffset (print 2.).




The output voltage of the amplifier is 5 V (print 3.)




Does anyone have experience with this?

Thank you
Best reagrds
Michael