Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1863: Frequency response at 96/192kHz frame rate.

Part Number: PCM1863

What is the frequency response at 96kHz and 192kHz frame rates?

I need to know -3dB point before considering for a new design, and the data sheet only references a response out to 20kHz.

  • Hi Adam,

    Figure 19 shows the FFT at a 192kHz sample rate and an effective 60kHz bandwidth. The decimation filter passband is 0.454*fs so this ends at 43.5kHz for the 96kHz fs case. Is this for an ultrasonic application? What bandwidth are you looking to achieve?

    Best,

    Zak