Part Number: SRC4192
Other Parts Discussed in Thread: SRC4193
Hello,
1. As the datasheet shows RCKI input is required in Master mode, and RCKI is not needed at "Both Input and Output ports are Slave mode"
So, internal PLL can be clocked from LRCK or BCK in Slave mode. Is that correct?
2. /RDY become "L" when connect BCK and LRCK from input-side and output-side
However input-side BCK and LRCK is stopped, /RDY still keeps "L".
Is this right behavior?
We are expecting internal "Rate estimator" can not get Rate data in this condition, then /RDY should be "H".
Regards,
Mochizuki