Other Parts Discussed in Thread: TLV320AIC3254EVM-K
Hi,
I am having troubles getting I2S Dout output from the AIC3254.
I am using (2) of the TLV320AIC3254EVM-K eval boards; one configured as I2S master (driving BClk and WClk and Dout) to the other AIC3254 as I2S slave, (as shown in figure below).
The master uses MCK from the TAS1020, SW2-5 is ON, (low) and I2S bus driving outof J14, so SW2-4 is Off (or high).
The I2S slave, uses MCK and I2S from J14, (via ribbon cable from the master), so SW2-5 and SW2-4 are Off, (or high).
For register configuration, for the master I am using I2S as the primary interface and have set the WClk and BClk as outlputs. I see these 2 clock outputs but not DOut.
Any ideas or help would be appreciated.
Can I get a known-good configuration file (Is2 master) I could load into my master AIC3254 to verify DOut is functional?
Thank you kindly,
-Dennis