Hi There,
Is TLV320aic34 supports PDM digital mic thru GIPO1_x and GPIO2_x terninals? and i guess IOVDD is the high voltage level for GPIO1_x and GPIO2_x?
Thanks,
Eric
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi There,
Is TLV320aic34 supports PDM digital mic thru GIPO1_x and GPIO2_x terninals? and i guess IOVDD is the high voltage level for GPIO1_x and GPIO2_x?
Thanks,
Eric
Hi Collin,
Thanks for quick response. So, TLV320aic34 supports PDM digital mic right? Please confirm.
Eric
Yes, please review Section 9.3.24 Digital Microphone Connectivity of the datasheet. The app note below also provides information about the connections:

Hello,
Unused analog inputs should be AC coupled to GND through a ~0.47uF capacitor. They can be shorted together instead of having to use individual capacitors for each unused input.
Digital inputs need to be connected to VCC or GND, and should not be left floating.
Analog outputs can be left floating.