This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3105: Analog full-scale 0dB input voltage

Part Number: TLV320AIC3105

Dear Specialists,

My customer is considering TLV320AIC3105IRHBR and has a question.

I would be grateful if you could advise.

---

Regarding TLV320AIC3105IRHBR on the data sheet

8.3 Recommended Operating Conditions Analog full-scale 0-dB input voltage

(DR VDD1 = 3.3 V) → 0.63VRMS

8.5 Electrical Characteristics Input signal level (0 dB) → 0.707VRMS

The value is different.
Which is the analog input level that becomes 0 dBFS at the time of AD conversion?

On the other hand, TLV320AIC3107IRSBR datasheet, both are 0.707VRMS.

---

I appreciate your great help in advance.

Best regards,

Shinichi