This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
Is it possible to use USB2ANY for controlling the PCM1753 by SPI?
Ito
Hi Ito,
Yes, the USB2ANY features SPI pins and can be controlled via PC using the USB2ANY Explorer software. You would just need to bring out the SPI lines from the connector. Note that the USB2ANY only supports 3.3V logic, but that should be okay with the PCM1753-Q1.
Thanks,
Paul