Part Number: TAS5805M
Other Parts Discussed in Thread: TAS5805
Hi Sirs,
We see harmonic distortion with the TAS5805 with 16bit I2S with 16kHz sample rate, while there is no problem with 32kHz, 44.1kHz, 48kHz, 88.2kHz, and 96kHz sample rates. Does this device support 16kHz sample rate? Customer is going to use PBTL mode in this case.
Distortion with 16kHz sample rate
Normal with 32kHz~96kHz sample rates
----------------------------------------------------------------
# Reset TAS5805_TAS5806
w 5a 00 00
w 5a 7f 00
w 5a 03 02
w 5a 01 11
w 5a 46 01
w 5a 03 02
d 05
# Register Tuning
w 5a 30 00
# Config DAC Gain to -12 dB
w 5a 4c 48
# Ramp Up / Down 0.5dB every 4FS
w 5a 4e bb
w 5a 4f b0
# Fsw=384kHz,1SPW mode, PBTL
w 5a 02 05
# Wake TAS5805_TAS5806
w 5a 03 03
w 5a 78 80
----------------------------------------------------------------
Thank you and Best regards,
Wayne Chen
11/09/2020