Part Number: LM48511
I am planning on using an external power supply for system architectural reasons. In review of the data sheet, I see that LSGND is the H-bridge ground and REGGND is the ground for the boost supply.
What is the recommended scheme for grounding when using an external boost power source. I am thinking that REGGND is not going to be carrying much, if any, current and I should tie the external power source ground directly to the LSGND pins to keep the loop tight. I would connect the REGGND and Signal Ground pins along with LSGND in a star, as the datasheet recommends.
In a related question, the application guide shows a 10uF bulk capacitor connected to the Vdd supply input and the inductor.. There are also several 1 uF capacitors on Vdd. With an eternal boost, can the 10uF capacitor be moved to the external regulator circuit?
Thanks,
Matt