Part Number: AIC111
Other Parts Discussed in Thread: TLV320AIC3204, TLV320AIC3100
Hi team,
There are two temperature parameters in AIC111 specification, one is operating free air temperature range: 0 ~ 70 ℃, and the other is functional temperature range: - 15 ~ 85 ℃. How are these two parameters defined and what are the differences? If AIC111 is used at - 15 ℃, what conditions are needed?