Other Parts Discussed in Thread: PCM1794A
Hello Sir,
One of my customer gona to use 2pcs PCM1795 to achieve 4CH output. Could you help to check their connection?
TDMCA mode can transfer both control signal and audio signal. Does it mean under TMDCA mode, PCM1795 register can be visited?
Shown as below block diagram, LRCK, BCK, SCK are used by both PCM1795s. If the second PCM1795's DI connected together and used to transfer control signal and audio data. DO feedback MCU's data and is connected together as well. the 1st PCM1795's DCO is connected to the second PCM1795's DCI.
If you have more material to talk about 2 pcs PCM1795 used in parallel. Please send for me the material.
Many thanks for your help!