Part Number: LM1875
Other Parts Discussed in Thread: LM384
Hi Team,
My customer's use case is input signal is 0~2.5V sine, frequency 5Khz, DC offset is 1.25V. Can LM1875 support this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Holly,
Yes, LM1875 can support it.
Regards,
Derek
Can LM384 also support this kind of input?LM1875 is 20W while customer only need 5W.
Hi Holly,
LM384 only support +-0.5V input.
Does customer consider Class-D amplifier? For 5W application, I suggest TPA3138, TPA3113.
They can get more technical support.
Regards,
Derek
Hi Derek,
To TPA3138, TPA3113, can the input signal phase difference 180 degrees?
Hi Holly,
TPA3138 and TPA3113 have two channels, and each channel is independent. So the two channels input signal phase can have 180 degree pahse.
Regards,
Derek