Part Number: PCM6340-Q1
Hi team,
Could you share me the characterization data of MicBias regulator in PCM6340-Q1?
Since (HVDD - MicBias) is small in my use case, I concerns how MicBias behaves If the recommended condition (HVDD>MicBias+0.6V) is violated.
I need following information under the condition below.
Condition : HVDD = 9V(typ), MicBias=8V setting, Load current = maximum 90mA,
DC-Coupled / R1=680ohm / Single end
#1.dropout performance at load current = 90mA
- HVDD vs MicBias plot (Y axis = MicBias voltage, X axis = HVDD(0V to 10V) )
- Dropout voltage(mV) vs. load current(0mA to 90mA)
#2. PSRR data (HVDD to MicBias)
regards,