This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1789: Can PCM1789 PIN18/19/24 float ?

Part Number: PCM1789


Dears:
Can PCM1789 PIN18,19,24 be left floating due to insufficient MCU resources? ?
And PIN17 AMUTEI pin uses a resistor to pull up in typical applications. Can this be removed? Thank you!
  • Hi Haiwen,

    Pin 18 and 19 can be left floating, as they are outputs. Pin 24 should be set to either ground or VDD, it should not be left floating.  If you are operating the device in HW mode, the pin should be connected to ground.

    Thanks,

    Paul