I use the device in PBTL mode to drive a transformer with only 30mOhms DC resistance of the primary. To prevent core saturation / asymmetrical magnetization I want to compensate the output offset voltage.
I found significant changes of the offset voltage if I hold a 1MOhm voltage probe of my oscilloscope at one of the inputs. Does it function to put a trim resistor (1MOhm) at both inputs tied with its tap to GND?
Another measure could be a xx kOhm resistor between the two inputs to minimize the input offset voltage. Would this improve the offset of the outputs?
Thanks in advance
Ulf