This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC6140: Connecting ADC input in parallel for 1/2 and 3/4 to use the 3dB improved DNR before DRE

Part Number: TLV320ADC6140

Is it possible to directly parallel the ADC Input's for 1/2 and 3/4 to use the 3dB improved DNR before DRE, using common DC blocking capacitors and other input circuitry?

  • Hello,

    Input channel summing is a supported feature in this device.  Take a look at Section 8.3.6.6 Programmable Channel Summer and Digital Mixer for more information.

    Yes, the inputs can be connected together after a common DC blocking capacitor for each of the pairs that are being summed.