Part Number: PCM1690-Q1
Hello Team,
I got question from customer as below. Can you please provide answer?
Q1. Can you please let me know the min/max value of internal pull-down resistor of LRCK, BCK, RST, MS/ADR0/RSV pins? This is because in the customer's circuit these pins are connected with their audio DSP. The DSP has internal pull-up resistor so they want to know the pull-down resistors' min/max value.
Q2. Regarding with BCK, LRCK pin, Can they put 2,2kohm or 4.7kohm pull-up resistor for external of these pin?
Q3. Datasheet recommend the VCOM capacitor is 10uF. In case customer changes the capacitance, what's happen?
Q4. In the customer's circuit, the sequence is below. The RST is firstly pull-up but will be pull-down for longer than 100ms. After that The SCKI is input. Is this sequence any problem?
Thanks,
Yuta Kurimoto