This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1802: whether the device can support 4.5V VCC?

Part Number: PCM1802
Other Parts Discussed in Thread: PCM1804

Hi, Team

since AKM is fire, our customer prefer to use PCM1802 replacing AK5381.

Since this is a MP project, so they must to keep the same VCC rail as before. And the VCC should be 4.5-4.6V in customer's SCH.

but form our PCM1802, our VCC is only 5V.

we also check our PCM1804, the PCM1804 VCC range is from 4.75-5.25.

Do u have any suggestions? customer needs to select a device that support 4.5V VCC.

Thanks.

G.W