Part Number: PCM1808
Hi team,.
Customer input clock, which is generated by crystal, to SCKI and the input will be Hi-Z during stop.
Do they need pull up or pull down resister?
if so, could you give me proper value?
LRCK and BCK of this device is Schmitt triger input with 50kohm pull down resister in slave mode.
When system clock is stopped and this device is master mode, is the output of LRCK and BCK High level?
Best regards,
Koyo