This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1808-Q1: rise time / fall time of SCKI

Part Number: PCM1808-Q1


Hi team,

I plan to use PCM1808-Q1 slave mode system clock = 12.288MHz (48khz, 256fs).

Could you give me the rise time and fall time requirement for this clock input?

regards,

  • Hello,

    Provided the minimum pulse-durations and duty cycles are abided by then a standard logic buffer or MCU GPIO pin will work fine.  The overall Audio Serial Interface (SCKI, BCLK, LRCLK) has maximum rise/falls times of 20ns as stated in Figures 22 and 23.