Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV135: Issue with 400Hz sine input using DRV135

Part Number: DRV135

Hello,

I'm using DRV135 to convert 400Hz single end input to differential output.

Attached schematics wherein I'm feeding  +/- 6.5VRms input to DRV and trying to convert singled end signal to differential signal for better noise immunity.

But unfortunately the I'm not able observe any output. I have an 5k load at the receiving end. I was trying to check the output waveform across 5K load. 

Appreciate if you can suggest whether 400Hz singled end input can be used with  DRV135 and convert it into differential o/p and check if there is any issues with the circuit

Best Regards,

Phani.M