Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LME49724: Encrypted TINA model - two versions

Other Parts Discussed in Thread: PCM1792A, LME49724

I was puttering along using this device as an output differential transimpedance stage for a PCM1792A, there is a bit of content error in the product folder model - but first, here is what is in the TINA V11 library

But the web folder model says to look at the header for modeled terms, but that is all missing in this model - so that comment to look at the header needs to go away, or the web folder model should add the header that is in the TINA library model, 

  • Hi, Michael,

    Thank you for the details you provided. We will take a look at it and will provide an answer as soon as possible.

    Best regards,
    Luis Fernando Rodríguez S.

  • Hi Michael,

    We will update LME49724 TINA Reference Design in order to show the modeled parameters.

    You can also check these at the unencrypted PSpice model and TINA model (module only) available in the same section of LME49724 product folder.
    The modeled parameters are the same across all models available.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators