Part Number: SRC4190
Hi,
I have some questions about SRC4190 when it is in Slave-Slave (input and output both slave) mode:
- It needs a reference clock (pin RCKI) even if it operates in Slave-Slave mode, right?
- What is the requirement of RCKI? (from datasheet it only say min: 128xfs max: 50 MHz)
- When in Slave-Slave mode, does RCKI need to be multiply of fs (128xfs/256xfs/512fs)? In this case, the fs is the input or output fs?
Thanks.
Gim Song