Part Number: PCM5122
Hi,
My customer is evaluating PCM5122A and Auto Clock Configuration doesn't work well.
The followings are present settings;
- Fs=44.1kHz
- BCK=11.28MHz(256fs)
- SREF[2:0]=001 (BCK)
- DCAS=0 (Auto)
・Clock Detector Status, Clock Status
- CDST=1001100 (SCK is missing, FS SCK ratio is invalid, SCK invalid)
- LTSH=1, CERF=1
The device works well on the following manual setting.
- DCAS=1 (Manual)
- P=2,J=16,D=0,R=1
- DDSP=2,DDAC=4,DNCP=4,DOSR=8,
- IDSK=1,IDCH=1
Do they miss any register settings?
Best Regards,
Kuramochi