Part Number: PCM5242RHBEVM
Other Parts Discussed in Thread: PCM5242
Hello, I hope someone can help me out.
Using the PCM5242 EVAL board.
Example 1; Loading the HybridFlow 4 and using the USB input, when I adjust the Biquads under Audio Processing it works fine. For example; a Linkwitz Low Pass, set at 100Hz. I get the expected results acoustically.
Example 2; Then change to the Optical input and move the jumper, sample rate 44.1kHz. When I set the same Low pass filter, I get full range output. The Low Pass filter does not change the audio output anymore.
Is there a step I'm missing to make it work? Also I would say Pure Path 2 console and the PCM5242 EVAL board using example 1 does not really seem stable on my computer as well. It has locked up a couple of times.
On a unrelated note....Pure Path 3 console and the supported EVAL boards for that which I have used, works fine.