Other Parts Discussed in Thread: TAS6424, TAS5414
Hi,
I am looking for a Speaker Amplifier with the specifications below.
- Rating : Automotive
- Operating Voltage : 3.3V~5V
- Input type : Digital input(I2S) & Analog input
- Architecture : Class-D
- Speaker Channels(output) : 2 channels(Stereo), with Headphone L/R
- Output Power : 5W or more
If there is a Speaker Amplifier that satisfies the above specs, please answer.