Hi,
I'm a complete novice at this topic, so please forgive me the intrusion, but TI Technical Support directed me to this forum, because my question was "too technical." Really?
Here goes...
I have purchased a Meier Audio Corda Stepdance headphone amplifier that uses the OPA1611. See: http://www.meier-audio.homepage.t-online.de/stepdance.htm
When I asked the amp's designer, Dr. Jan Meier, the questions below, he directed me to this datasheet for the OPA1611: http://focus.ti.com/lit/ds/symlink/opa1611.pdf
I've attempted to interpret the datasheet for this opamp with the goal of figuring out how many Watts (or milliwatts) RMS (or even just peak Watts) the opamp can produce with a given supply voltage (Vs).
If I'm interpreting the specs correctly, specifically Figures 4 and 27, with a supply voltage (Vs) of +/-15V, at 25-degrees C, the maximum output voltage (Vppp) is about 28.5V across all audible frequencies (Figure 4) and the maximum output current will be about 47 mA.
Question #1:
Would it be correct to calculate the maximum (peak?) output Watts as follows?:
Max Output Voltage (Vppp) * Max Output Current (mA) = Max Output Watts
28.5V * 47mA = 1339.5 mW (at 25-degrees C, with a +/-15V supply voltage)
If not, can someone please correct my math (and/or my interpretations/assumptions)?
Question #2:
From reading elsewhere on the net, I understand that Watts RMS could be calculated as 0.707 * Peak Watts if only the signals were pure sine waves, which for audio amps is not the case, of course.
Can someone give a ballpark way of estimating Watts RMS (into 50-ohm headphones) when Peak Watts is known (if indeed I've calculated it correctly)?
Question #3:
Lastly, since the OPA1611's Output Voltage varies with the Supply Voltage, given that my headphone amplifier allows external supplies to range from 6VDC to 15VDC -AND- given that the amp designer has included a circuit that doubles the voltage coming from the external supply, as if a PSU that supplies 15VDC was actually supplying 30VDC, would I have to use a 7.5VDC external linear regulated power supply to mimic the conditions documented in Figures 4 and 27? In other words, when the datasheet specifies a Supply Voltage (Vs) of +/-15V, would that be what I'm supplying with a 7.5VDC PSU (given that the amp's design doubles the supply voltage)?
Along those lines, given that the amplifier's specs indicate users can connect PSU's that supply anywhere from 6VDC to 15VDC, how can there be a voltage-doubling circuit if the OPA1611's Supply Voltage must fit the range +/-2.25V to +/-18V?
Thank you in advance!
Mike