Part Number: PCM2901
Dear Sir:
When I tested the function of PCM2901E, I found that there was a noise when I entered the system or entered the desktop with password.I tested Ubuntu 16.04/18.04/20.04 and found this noise,but it was not found in WIN10. After entering the OS, the audio function is OK.
Test platform: Intel APL N3350 + PCM2901E
This is a USB waveform that does not play audio files after entering the system:
This is the USB waveform in case of noise or playing audio files or hot plug codec chips while the system is running:
So the source of the noise is the data on the USB waveform. But for a voice data, why does it become noise after codec conversion? Is there any way to avoid this noise?
Looking forward to your help,thanks.
Long.zhang