Other Parts Discussed in Thread: PCM6260-Q1, PCM6240-Q1
Hi, Expert
My customer is asking how does PCM6260 TDM support 73.728 Mhz
384kHz×32bits×6ch=73.728MHz
Out put to external Audio chip via SDOUT TDM.
Your advice is appreciate
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Expert
My customer is asking how does PCM6260 TDM support 73.728 Mhz
384kHz×32bits×6ch=73.728MHz
Out put to external Audio chip via SDOUT TDM.
Your advice is appreciate
Hello Takeshi-san,
First, the maximum BCLK frequency of the PCM6xx0-Q1 family is 25MHz (40ns min period - Section 7.10 in datasheet).
Second, there are limited processing resources available in the PCM6xx0-Q1 family to perform the required decimation and filtering at higher speeds and as a result the maximum channel count while operating at 384kHz is 2. Please find more information about the supported combinations in the following application note:

Hi Collins,
If 384kHz limit the maximum number of channel to be processed to 2 channels,
Even if I limit the resolution to 16bit (384kHz x 16bit x 4 = 24.5MHz), the maximum output channel is still limited to 2 channels?
regards,
Hello,
The maximum channel count is related to internal processing requirements from the fixed resource processing engine performing the decimation, filtering, DRE/AGC, etc. Therefore, the data length and resulting max BCLK frequency is not the limiting factor.
We've been communicating offline directly and we've shown that it's actually possible (barely) to get 3 active channels using the PCM6260-Q1 or PCM6240-Q1 at 384kHz sampling rates provided soft-stepping and most other processing features are turned off while using the three channels.