Part Number: PCM1789
Hi Team,
Would you advise about my customer inquiry that
1, There is below description on page 3 in PCM1789-Q1 datasheet but no description in PCM1789 datasheet. Is this common for both devices?
(1) BCK and LRCK (Schmitt trigger input with 50-kΩ typical internal pull-down resistor).
(2) DIN (Schmitt trigger input).
(3) SCKI, ADR5/ADR1/RSV, MC/SCL/FMT, MD/SDA/DEMP, and AMUTEI (Schmitt trigger input, 5-V tolerant).
(4) RST and MS/ADR0/RSV (Schmitt trigger input with 50-kΩ typical internal pull-down resistor, 5-V tolerant).
(5) ZERO1 and ZERO2.
(6) AMUTEO and SDA (I2C mode, open-drain low output).
2. My customer use PCM1789 with hardware control mode. please advise below connection no problem?
① Are 18pin ZERO2/AMUTEO and 19pin ZERO1 open no problem?
② Can the customer connect 23pin(MS/ADR0/RSV) and 24pin(ADR5/ADR1/RSV) to GND directly?
Thanks
Best regards,
Shidara