Hi,
I had buy TLV320AIC34EVM to develop ENC and ANC, but I can not implement our own algorithm on TAS1020.
Can you provide the SDK or sample firmware of TAS1020 to me for development. Thanks.
Jim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I had buy TLV320AIC34EVM to develop ENC and ANC, but I can not implement our own algorithm on TAS1020.
Can you provide the SDK or sample firmware of TAS1020 to me for development. Thanks.
Jim
Hi Collin,
So, I can not control AIC34 through TAS1020?
There should be the SDK or something that I can compile it and download Bin file (binary code) to TAS1020.
Because the EVM-K is use TAS1020 to control AIC34.
Jim
Hi Jim,
The tools and source code for what's used on the EVM are no longer available. We are able to load a hex file into the TAS1020 during the EVM production but at this point it's a fixed system with no way to modify it.