Part Number: PCM5142
Other Parts Discussed in Thread: PCM3070
Hello, I am using PCM5142 recently. My requirement is that minidsp generates an interrupt signal and outputs it from the GPIO pin, or I can get the generated interrupt by reading the register.
I used it on PCM3070 well before, but PCM5142 doesn't have the same register allows me to configure which GPIO pin the interrupt output.
this is the pcm5142 pfw file
and this is the register of pcm3070 ,page 0 register 0x34
emm,,,,,am i clear enough?