Part Number: DRV135
Hi,
We used DRV135 in our design and I attached the schematic. For test the thermal performance, we add the output load resistors, these are used only simulation the end user. We have 2 type of usage, one is differential output and the load is 150 ohm, and the other is single ended with 600 ohm load. When we observe the temperature the DRV135 at room temperature and unboxed board. we saw the differential output version is about 90 C and single ended version is 120 C. These temperature values are too high for a unboxed free air medium at 25 C. Do these values normal for the DRV135? There are no exposed pad and to cool the IC is very problematic. Please check on your side and inform me , if is there any mistake on our design. And also could you please confirm me that DRV135 is fixed gain of 2? Am I right?