Part Number: TPA3255EVM
Other Parts Discussed in Thread: TPA3255
Hello,
I am testing TI evaluation module and I appreciate if you answer my following questions:
1- For BTL, with differential inputs, the jumper state is actually confusing considering the user guide, quick user guide and the comments in the TI support forums.
I am using XLR connector to connect AP to the input. What should be the state of jumper J21?
I actually tried with and without J21 and got the same results. Is that correct?
2- I tested BTL configuration, 4ohm loads, 1kHz input signal and at Vin=2.3Vrms, 430W output power (215W per channel) started to see clipping and the indicator LED was turned on at this point. Is it supposed to be like this? How can I increase the power without clipping? For 8ohm load the clipping started at about 200W output power (100W per channel).
3- Can we change the voltage gain of the TPA3255?