Part Number: TAS5754MDCAEVM
Is the TAS5754 development board compatible with the PPCMB Rev D? I have an older PPCMB that was used with the TAS5760 amp dev board. Plugged in the TAS5754 amp dev board and only some of the features are working. Dynamic EQ and PBE do not work. Volume controls work Ok. Using PPC2. When starting the program I get the below error. Selecting "connect as TAS5754"then sw communicates with the PPCMB. The following screen shows the TAS5754 features but the firmware shows TAS5760. Do I need a newer PPCMB or can I update the firmware on the PPCMB? If firmware can be updated what is the process?
Best