I would like to use PCM2904 as two channels acquisition device.
I have built the circuit according to the schematics shown in figure 38 of the datasheet.
I manage to acquire correctly the input VinL (pin 12). However, I don't see any signal acquired when the input is moved to the VinR pin.. In my circuit C9 and C10 are 100nF ceramic capacitors.
I am not clear if this behaviour depends on the default configuration descriptor. Is by default the chip configured to acquire only one channel?
Thanks in advance