Part Number: TAS5825M
Hi TI-team,
I'm working on an amplifier project with tas5825m. Test designs with that amp chip are up and running so far. Now I'm thinking of which process flow to choose.
The problem is, I need various features and there is no process flow which includes all that features. The features I definitely need:
- Hybrid modulation
- Delay
- Dynamic EQs
- AGL
- the option to use more filters for crossover instead of using so much filters for general eqing (for example in 1.1 mode)
Is it possible to combine features of various process flows? Can you give some information about the internal signal routing of the dsp core? With that information it would be possible to configure the needed features with the help of the datasheet.
Kind regards,
Markus