Part Number: TLV320DAC3100
Hello team,
In this application my customer is using HPL output as a line driver (600ohm) and also the power output to drive a 1W 8ohm speaker. The speaker is pre-wired inside a hand-held and one side is tied to ground, so only one side of it can be drived. How can we connect the class-D differential output to this speaker?
I guess we could connect both SPKP together and drive the speaker with it. In this case what should we do with both SPKM pins?
Do I need filters of DC-block in between SPKP pins and the speaker?
Also, as an extra question, there is any case where the MCLK is mandatory or we can always use BCLK and PLL to generate the internal clock?
Thank you!