Part Number: ADC6140EVM-PDK
Other Parts Discussed in Thread: TLV320ADC6140
HI
I would like to test the performance of the TLV320ADC6140 on the EV board, I'm using Purepath.
Everything works fine in slave mode, and my question is now, is it possible to set the EV board up in master mode, and run it with :
1channel.
Sampling rate: 96kHz
MCLK 24.576MHz
BCLK/FSYNC ratio: 32
I can do it with my microcontroller, but can I do it with purepath?
So i'm a little in doubt if I should add a 24,576MHz MCLK from an external device. hope you can help, thanks in advance.