Part Number: TPA3221
Hi,
I'm having an "starup" issue with my TPA3221 design. I run the amp as a 2ch stereo amp.
1. I have a bluethooth module that controls the RESET-pin. It has 3.3V level but that should be OK according to the datasheet as VIH = min 1.9V on the RESET-pin.
2. I control the CMUTE pin also from the same bluetootrh module. Also here with 3.3V-level which should be OK as VIH is also 1.9V for CMUTE-pin! Or am I wrong? The CMUTE-pin is kind of special as it charges an external cap to achieve a softer ramp up/down! So maybe I am doing something wrong here?
3. Note that VDD (5V) and PVDD (24V) are stable before I drive RESET high!
NOTE: NM = Not Mounted
The problem I have is the following:
Most of the times when I drive RESET high (3.3V) the amp does not start! I drive CMUTE high 400 ms after I have driven RESET high. Once I have even got one of the two channels (sma chip) to start but not the other one. When I say "does not start" I mean that the outputs from the amp is Hi Z!
Please help me understand what I am doing wrong here!Best regards
Markus