This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Are the analog power supplies of VCC1 and VCC2 connected internally?
Additionally, is my understanding correct that VCC1 is the anaog power supply for VOUT5+/- ~ VOUT8+/- and VCC2 is the analog power supply for VOUT1+/- ~ VOUT4+/- ?
Best regards,
Kato
Hi Kato-san,
Sorry I missed your question yesterday.
You are correct about the VCC pin and the supplied channels. I do not think they are connected directly together in the design, but they should be connected to the same potential on the PCB. They likely still have some higher impedance connection to each other, but I would not recommend only providing +5V to one pin.
Thanks,
Paul