Other Parts Discussed in Thread: CC8531, CC8520, DIR9001
I have problems in getting expected responses to some commands from master and slave.
First I establish a network that I check with NWM_GET_STATUS on master. Then I want to stream audio with NWM_ACH_SET_USAGE. I prepare the 16 1-byte parameters where only the first two are 0x0 and 0x1 then 0xFF. After execution of this command I do again NWM_GET_STATUS on themaster but both the ACH_USED in the conected slaves enumeration part and the ACH_USED in the main part bytes[3:4] show only zeros which suggests no slave streams audio while I issued the NWM_ACH_SET_USAGE command just a few moments before.
The second question is about datagrams where I am also unsuccessful so far - when I send a first datagram as I understand it should reset the connection setting the LSB in the first parameter of DSC_TX_DATAGRAM. Is the procedure that it has to be master who sends this reset connection datagram (length irrelevant and has to be e.g. 0 ?) or it can also be slave or they both have to exchange reset connection datagrams ? Should the slave get the EVT_DSC_RX_AVAIL flag set when the master has sent the reset connection intiating datagram ? That does not happen at me - the slave does not see the EVT_DSC_RX_AVAIL flag set - what can be wrong in my datagrams implemenetation and understanding ?
Best regards,
Pawel