Other Parts Discussed in Thread: TPA3244, TPA3245
Hello Expert,
I'm looking for lower power consumption device than TPA3156D2.
Detailed requirement specification is as follow.
・Input type: Analog or I2S
・Ch: 1ch BTL or 1ch PBTL
・PVDD: 24V
・Load: 2ohm or 4ohm
・Maximum output power: 150W peak(don't need to support 150W continuously)
Please let me know if there is more appropriate device for this opportunity.
By the way, I confirmed some audio amp datasheet including TPA3156D2.
Then some device has each power supply pin's power consumption(PVCC, DVDD, GVDD, etc) but TPA3156D2 datasheet only have Icc.
Would you tell me whether this Icc included all pin's current or it is only PVCC current?
If it is only for PVCC pin's power consumption, could you provide other pins typical idle current?
Best regards,
Kazuki Kuramochi